Part Number: ADS5295
Can you go into more detail regarding the PRBS function? The register seems to use 24-bits and the part is just 12-bits. How does this map to the outputs when the customer uses it? Does it map to how he sets up the interface? Is it exactly the same as how you set up the interface to operate? Can you please explain this is greater detail as I have a customer asking the following questions:
I am assuming the PRBS contains the pattern for serial to parallel alignment when programmed to do so. Is this correct? I noticed that this is a 23 bit pattern with a ‘0’ forced at bit 16, (1st bit after the 1st word of PRBS).
Does this repeat in a back to back fashion (the next clock edge after the last bit in the PRBS will be the 1st bit of the next PRBS stream)? Is the correct?
Am I understanding the PRBS function properly based on questions above?
Do we have a document that would explain this in even more detail?
Is there any detailed programming document for the ADS5295?
Thanks for your help with this!
Richard Elmquist