Other Parts Discussed in Thread: LMK04828, DAC37J84, DAC38J84
I need to access the SPI port of the LMK04828 on the DAC3XJ8X EVM board, but there's no direct connection via the FMC.
There is a header labelled "LMK SPI" (J25) but I don't see it referenced anywhere and it goes directly into the CPLD on the EVM.
Can someone tell me more about how J25 is connected to the on-board CPLD, or what I have to do to use J25, or provide me the CPLD code?
Thanks