Other Parts Discussed in Thread: ADS1292R
Tool/software: Code Composer Studio
Fellow I have some problems with a integration of ADS1292R with msp432, can anyone give me some help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ryan,
I am developing a prototype of electrocardiogram with recourse to the front end ads1292R, I bought the chip and started to assemble the entire circuit from root, I am using the msp432 micro controller. Now I am facing serious problems, I have already created the spi drivers, but I would like to have a functional example, or at least one guide line, to check the ads1292R communication with the microcontroller, I created a main file, but I do not know how call the ads1292R startup, or check conversion values. I send you my SPI files:
/***************************************************************** * INCLUDE * ******************************************************************/ #include <msp.h> #include "ads1292r.h" /***************************************************************** * GLOBAL VARIABLES * ******************************************************************/ unsigned char ADC_READ_DATA[16]; unsigned char ADS1292R_SPI_CMD_FLAG = 0; unsigned char ADS1292R_SPI_DATA_FLAG = 0; unsigned char SPI_SEND_COUNT = 0; unsigned char SPI_TX_COUNT = 0; unsigned char SPI_TX_BUFF[10]; unsigned char SPI_RX_DATA_FLAG = 0; unsigned char SPI_RX_BUFF[12]; unsigned char SPI_RX_COUNT = 0; unsigned char SPI_RX_EXP_COUNT = 0; unsigned char ECG_DATA_READY; long ADS1292R_ECG_DATA_BUFF[6]; /*DEFINE RECORD STATE OF ECG*/ /**/ #define DELAY_COUNT 2 extern struct ADS1292R_STATE ecg_Record_State; extern unsigned char ECG_RECORD_DATA_BUFFER[256], RECORD_H; unsigned char ADS1292R_REGVAL[16] = { /*DEVICE ID*/ 0x00, /*CONFIG1*/ 0x02, /*CONFIG2*/ 0xE0, /*LOFF*/ 0xF0, /*CH1SET (PGAIN = 6)*/ 0x00, /*CH2SET (PGAIN = 6)*/ 0x00, /*RLD_SENS (DEFAULT)*/ 0x2C, /*LOFF_SENS (DEFAULT)*/ 0x0F, /*LOFF_STAT*/ 0x00, /*RESP1*/ 0xEA, /*RESP2*/ 0x03, /*GPIO*/ 0x0C }; unsigned char ADS1292R_DEFAULT_REGISTERS_SETTINGS[15] = { /*DEVICE ID*/ 0x00, /*CONFIG1*/ 0x02, /*CONFIG2*/ 0xE0, /*LOFF*/ 0xF0, /*CH1SET (PGAIN = 6)*/ 0x00, /*CH2SET (PGAIN = 6)*/ 0x00, /*RLD_SENS (DEFAULT)*/ 0x2C, /*LOFF_SENS (DEFAULT)*/ 0x0F, /*LOFF_STAT*/ 0x00, /*RESP1*/ 0xEA, /*RESP2*/ 0x03, /*GPIO*/ 0x0C }; /***************************************************************** * VARIABLES FOR SPI INTERATION * ******************************************************************/ void ads1292R_Clock_Select(unsigned char clock){ if(clock == 1){ P4->OUT |= (enum PORT4_ADC_CONTROL)ADC_CLK_SEL; }else{ P4->OUT &= ~(enum PORT4_ADC_CONTROL)ADC_CLK_SEL; } } /**********ADS1292R RESET**********/ void ads1292R_Reset(void){ unsigned short i; P3->OUT |= (enum PORT3_ADC_CONTROL)ADC_RESET; /*SET PIN TO HIGH*/ /*PROVIDE A DELAY*/ for( i = 0; i < 5000; i++); /*WAIT SOME TIME*/ P3->OUT &= ~(enum PORT3_ADC_CONTROL)ADC_RESET; /*SET PIN TO LOW*/ for( i = 0; i < 5000; i++); /*WAIT SOME TIME*/ P3->OUT |= (enum PORT3_ADC_CONTROL)ADC_RESET; /*SET PIN TO HIGH*/ for( i = 0; i < 35000; i++); } /**********ADS1292R DISABLE START**********/ void ads1292R_Disable_Start(void){ unsigned short i; P3->OUT &= ~(enum PORT3_ADC_CONTROL)ADC_START; /*SET PIN TO LOW*/ /*PROVIDE A DELAY*/ for( i = 0; i < 35000; i++); /*SMALL DELAY*/ } /**********ADS1292R ENABLE START**********/ void ads1292R_Enable_Start(void){ unsigned short i; P3->OUT |= (enum PORT3_ADC_CONTROL)ADC_START; /*SET PIN TO HIGH*/ /*PROVIDE A DELAY*/ for( i = 0; i < 50000; i++); /*SMALL DELAY*/ } /**********ADS1292R CHIP ENABLE**********/ void ads1292R_ChipSet_Enable(void){ /*ADS1292R CS PIN IS IN ACTIVE LOW*/ P3->OUT &= ~(enum PORT3_ADC_CONTROL)ADC_CS; /*SET TO LOW*/ } /**********ADS1292R CLEAR CHIP ENABLE**********/ void ads1292R_ChipClear_Enable(void){ unsigned char CsDelay; for(CsDelay = 0; CsDelay <100; CsDelay++); /*ADS1292R CS PIN IS IN ACTIVE LOW*/ P3->OUT |= (enum PORT3_ADC_CONTROL)ADC_CS; /*SET TO HIGH*/ } /**********ADS1292R DRDY INTERRUPT**********/ void ads1292R_DRDY_Interrupt(void){ P2->DIR &= ~0x02; P2->REN |= BIT5; /*ENABLE P2.5 INTERNAL RESISTANCE*/ P2->OUT |= BIT5; /*SET P2.5 AS PULL-UP RESISTANCE*/ P2->IES |= BIT5; /*P2.5 LO/HI EDGE*/ P2->IFG &= ~BIT5; /*P2.5 IFG CLEARED*/ P2->IE &= ~BIT5; /*P2.5 INTERRUPT DISABLE*/ } /**********ENABLE ADS1292R DRDY INTERRUPT**********/ void Enable_ads1292R_DRDY_Interrupt(void){ P2->IFG &= ~BIT5; /*P2.5 IFG CLEARED*/ P2->IE |= BIT5; /*P2.5 INTERRUPT ENABLE*/ } /**********DISABLE ADS1292R DRDY INTERRUPT**********/ void Disable_ads1292R_DRDY_Interrupt(void){ P2->IFG &= ~BIT5; /*P2.5 IFG CLEARED*/ P2->IE &= ~BIT5; /*P2.5 INTERRUPT ENABLE*/ } void Set_ads1292R_GPIO(void){ P4->SEL0 = 0x00; P4->DIR |= 0x8F; P4->OUT |= (enum PORT4_ADC_CONTROL)POW_CE; P3->DIR |= 0x07; P3->OUT &= 0xF8; P3->OUT |= (enum PORT3_ADC_CONTROL)ADC_CS; // Set RESET, START to Low and CS to High P3->OUT |= (enum PORT3_ADC_CONTROL)ADC_RESET; // Set RESET, START to Low and CS to High P4->OUT = 0x03; //dataCnt = 0; // P1.1 interrupt disabled } /**********SET ADS1292R UCB0_SPI**********/ void Set_ads1292R_UCB0_SPI(void) { P3->SEL0 |= BIT5 | BIT6 | BIT7; /*SET 3 PIN SPI PERIPHERAL BITS*/ P3->DIR |= BIT5 | BIT6; /*CLOCK AND DIROUT AS OUTPUT*/ P3->DIR &= ~BIT7; /*DIN AS INPUT*/ EUSCI_B0->CTLW1 |= EUSCI_B_CTLW0_SWRST; /*ENABLE SW RESET*/ EUSCI_B0->CTLW0 |= EUSCI_B_CTLW0_MSB | EUSCI_B_CTLW0_MST | EUSCI_B_CTLW0_SYNC; //[b2-1] 00- 3-pin SPI //[b3] 1 - Master mode //[b4] 0 - 8-bit data //[b5] 1 - MSB first //[b6] 0 - Clock polarity low. //[b7] 1 - Clock phase - Data is captured on the first UCLK edge and changed on the following edge. EUSCI_B0->CTLW1 |= TASSEL__ACLK; // ACLK UCB0BR0 = 24; // 1 MHz UCB0BR1 = 0; // EUSCI_B0->CTLW1 &= ~EUSCI_B_CTLW0_SWRST; /*CLEAR SW RESET, RESUME OPERATION*/ } /**********SET ADS1292R DMA**********/ void Set_DMA_SPI(void) { DMACTL0 = DMA0TSEL_12; // USCI_B0 Transmit Ready Trigger //DMA0SA = (void (*)())&UCB0RXBUF; // Source block address //DMA0DA = (void (*)())ADC_Read_data; // Destination single address DMA0SZ = 16; // Block size DMA0CTL = DMADT_4 + DMADSTINCR_3 + DMADSTBYTE + DMASRCBYTE; // Rpt, inc src, byte-byte DMA0CTL |= DMAEN; // Enable DMA for consecutive Xfers } /**********ADS1292R SPI COMMAND DATA**********/ void ads1292R_SPI_Command_Data(unsigned char data_in){ unsigned char delayVar; ads1292R_ChipSet_Enable(); for(delayVar = 0; delayVar < 50; delayVar++); ads1292R_ChipClear_Enable(); ads1292R_ChipSet_Enable(); EUSCI_B0->TXBUF = data_in; while((EUSCI_B0->IFG & EUSCI_B_IFG_RXIFG0)); delayVar = EUSCI_B0->RXBUF; for (delayVar = 0; delayVar < 150; delayVar++); } /**********ADS1292R WAKE UP**********/ void ads1292R_WakeUp(void){ ads1292R_SPI_Command_Data(WAKEUP); /*SEND WAKE UP COMMAND */ } /**********ADS1292R SLEEP**********/ void ads1292R_Sleep(void){ ads1292R_SPI_Command_Data(STANDBY); /*SEND STANDBY COMMAND */ } /**********ADS1292R SOFT START**********/ void ads1292R_Soft_Start(void){ ads1292R_SPI_Command_Data(START); /*SEND START COMMAND */ ads1292R_ChipClear_Enable(); } /**********ADS1292R START/RE-START**********/ void ads1292R_HardReStart(void){ P3->OUT |= (enum PORT3_ADC_CONTROL)ADC_START; } /**********ADS1292R SOFT RESET**********/ void ads1292R_Soft_Reset(void){ ads1292R_SPI_Command_Data(RESET); /*SEND RESET COMMAND */ } /**********ADS1292R SOFT STOP**********/ void ads1292R_Soft_Stop(void){ ads1292R_SPI_Command_Data(STOP); /*SEND STOP COMMAND */ } /**********ADS1292R HARD STOP**********/ void ads1292R_Hard_Stop (void){ unsigned short i, j; P3->OUT &= ~(enum PORT3_ADC_CONTROL)ADC_START; /*SET START PIN TO LOW*/ for (j = 0; j < DELAY_COUNT; j++){ for ( i=0; i < 35000; i++); } } /**********ADS1292R START READ CONTINUOUS**********/ void ads1292R_Start_Read_Data_Continuous (void){ ads1292R_SPI_Command_Data(RDATAC); } /**********ADS1292R STOP READ CONTINUOUS**********/ void ads1292R_Stop_Read_Data_Continuous (void){ ads1292R_SPI_Command_Data(SDATAC); } /**********ADS1292R START DATA CONVERTION COMMAND**********/ void ads1292R_Start_Data_Conv_Command (void){ ads1292R_SPI_Command_Data(START); } /**********ADS1292R INITIALIZATION**********/ void ads1292R_Init(void){ ads1292R_Reset(); ads1292R_Disable_Start(); ads1292R_Enable_Start(); } /**********ADS1292R ENABLE CONVERTION**********/ void ads1292R_EnableConvertion(void){ ads1292R_Start_Read_Data_Continuous(); ads1292R_HardReStart(); } /**********ADS1292R REGISTERS WRITE**********/ void ads1292R_Reg_Write(unsigned char READ_WRITE_ADDRESS, unsigned char DATA){ short y; switch(READ_WRITE_ADDRESS){ case 1: DATA = DATA & 0x87; break; case 2: DATA = DATA & 0xFB; DATA |= 0x80; break; case 3: DATA = DATA & 0xFD; DATA |= 0x10; break; case 7: DATA = DATA & 0x3F; break; case 8: DATA = DATA & 0x5F; break; case 9: DATA |= 0x02; break; case 10: DATA = DATA & 0x87; DATA |= 0x01; break; case 11: DATA = DATA & 0x0F; break; default: break; } SPI_TX_BUFF[0] = READ_WRITE_ADDRESS | WREG; SPI_TX_BUFF[1] = 0; /*WRITE SINGLE BYTE*/ SPI_TX_BUFF[2] = DATA; /*WRITE SINGLE BYTE*/ ads1292R_ChipSet_Enable(); for ( y = 0 ; y < 50; y++); EUSCI_B0->TXBUF = SPI_TX_BUFF[0]; /*SEND THE FIRST DATA TO TX BUFFER*/ while((EUSCI_B0->IFG & EUSCI_B_IFG_RXIFG0)); /*EUSCI_B0_ TX READY?*/ y = EUSCI_B0->RXBUF; /*READ RX BUFF*/ EUSCI_B0->TXBUF = SPI_TX_BUFF[1]; /*SEND THE FIRST DATA TO TX BUFFER*/ while((EUSCI_B0->IFG & EUSCI_B_IFG_RXIFG0)); /*EUSCI_B0_ TX READY?*/ y = EUSCI_B0->RXBUF; /*READ RX BUFF*/ EUSCI_B0->TXBUF = SPI_TX_BUFF[2]; /*SEND THE FIRST DATA TO TX BUFFER*/ while((EUSCI_B0->IFG & EUSCI_B_IFG_RXIFG0)); /*EUSCI_B0_ TX READY?*/ y = EUSCI_B0->RXBUF; /*READ RX BUFF*/ } /**********ADS1292R REGISTERS READ**********/ unsigned char ads1292R_Reg_Read (unsigned char READ_ADDRESS){ unsigned char retVal; /*RETURN VALUE*/ SPI_TX_BUFF[0] = READ_ADDRESS | RREG; SPI_TX_BUFF[1] = 0; /*READ BYTE NUMBER -1*/ ads1292R_ChipSet_Enable(); /*SET CHIP SELECT TO LOW*/ EUSCI_B0->TXBUF = SPI_TX_BUFF[0]; /*SEND THE FIRST DATA TO TX BUFFER*/ while((EUSCI_B0->IFG & EUSCI_B_IFG_TXIFG0)); /*EUSCI_B0_ TX READY?*/ EUSCI_B0->TXBUF = SPI_TX_BUFF[1]; /*SEND THE FIRST DATA TO TX BUFFER*/ while((EUSCI_B0->IFG & EUSCI_B_IFG_RXIFG0)); /*EUSCI_B0_ TX READY?*/ retVal = EUSCI_B0->RXBUF; /*READ RX BUFFER*/ EUSCI_B0->RXBUF = 0x00; /*SEND FIRST DATA TO THE TX BUFFER*/ while((EUSCI_B0->IFG & EUSCI_B_IFG_RXIFG0)); /*EUSCI_B0_ TX READY?*/ retVal = EUSCI_B0->RXBUF; /*READ RX BUFFER*/ ads1292R_ChipClear_Enable(); /*DISABLE CHIP SELECT*/ return retVal; /*RETURN THE VALUE*/ } /**********ADS1292R DEFAULT REGISTERS INITIALIZATION**********/ void ads1292R_DefaultReg_Init(void){ unsigned char regInit; ads1292R_ChipSet_Enable(); for(regInit = 0; regInit<100; regInit++); ads1292R_ChipClear_Enable(); if((ADS1292R_REGVAL[0] & 0x20 )==0x20){ for(regInit = 1; regInit<12;regInit++){ ads1292R_Reg_Write(regInit, ADS1292R_DEFAULT_REGISTERS_SETTINGS[regInit]); } }else{ for(regInit = 1; regInit<12;regInit++){ ads1292R_Reg_Write(regInit, ADS1292R_DEFAULT_REGISTERS_SETTINGS[regInit]); } } } /**********ADS1292R READ ALL REGISTERS**********/ void ads1292R_ReadAll_Reg(unsigned char ADS1292R_BUFF[]){ unsigned char AllReg_i; ads1292R_ChipSet_Enable(); for(AllReg_i = 0; AllReg_i<200; AllReg_i++); ads1292R_ChipClear_Enable(); for(AllReg_i = 0; AllReg_i<12; AllReg_i++){ ADS1292R_BUFF[AllReg_i] = ads1292R_Reg_Read(AllReg_i ); } } /**********ADS1292R POwer INIT**********/ void ads1292R_PowerOn_Init(void){ volatile unsigned short ini_i, j; ads1292R_InitResource(); ads1292R_Reset(); for(j=0; j<DELAY_COUNT;j++){ for(ini_i = 0; ini_i < 20000; ini_i++); for(ini_i = 0; ini_i < 20000; ini_i++); for(ini_i = 0; ini_i < 20000; ini_i++); } ads1292R_DRDY_Interrupt(); ads1292R_Clock_Select(1); /*SET INTERNAL CLOCK*/ for(ini_i = 0; ini_i < 20000; ini_i++); for(ini_i = 0; ini_i < 20000; ini_i++); for(ini_i = 0; ini_i < 20000; ini_i++); ads1292R_Disable_Start(); ads1292R_Enable_Start(); ads1292R_Hard_Stop(); ads1292R_Start_Data_Conv_Command(); ads1292R_Soft_Stop(); for(j=0; j<DELAY_COUNT;j++){ for(ini_i = 0; ini_i < 20000; ini_i++); } ads1292R_Stop_Read_Data_Continuous(); for(j=0; j<DELAY_COUNT;j++){ for(ini_i = 0; ini_i < 35000; ini_i++); } for(j=0; j<DELAY_COUNT;j++){ for(ini_i = 0; ini_i < 35000; ini_i++); } ads1292R_ReadAll_Reg(ADS1292R_REGVAL); ads1292R_DefaultReg_Init(); ads1292R_ReadAll_Reg(ADS1292R_REGVAL); } void ads1292R_Parse_DataPacket(void){ unsigned char ecg_chan_num; switch(ecg_Record_State.state){ case DATA_STREAMING_STATE: { for(ecg_chan_num = 0; ecg_chan_num < 3; ecg_chan_num++){ ADS1292R_ECG_DATA_BUFF[ecg_chan_num] = (signed long)SPI_RX_BUFF[3*ecg_chan_num]; ADS1292R_ECG_DATA_BUFF[ecg_chan_num] = ADS1292R_ECG_DATA_BUFF[3*ecg_chan_num] << 8; ADS1292R_ECG_DATA_BUFF[ecg_chan_num] |= SPI_RX_BUFF[3*ecg_chan_num+1]; ADS1292R_ECG_DATA_BUFF[ecg_chan_num] = ADS1292R_ECG_DATA_BUFF[3*ecg_chan_num] << 8;; ADS1292R_ECG_DATA_BUFF[ecg_chan_num] |= SPI_RX_BUFF[3*ecg_chan_num+2]; } } break; case ACQUIRE_DATA_STATE: case ECG_RECORDING_STATE: { unsigned char *ptr; ptr = &ECG_RECORD_DATA_BUFFER[RECORD_H << 3]; /*POINT TO CIRCULAR BUFFER AT HEAD*8 */ *ptr++ = SPI_RX_BUFF[0]; /*STORE STATUS*/ *ptr++ = SPI_RX_BUFF[1]; /*STORE STATUS*/ /*SPI_RX_BUFF IS ALWAYS 0x00 DO IT IS DISCARDED*/ *ptr++ = SPI_RX_BUFF[3]; /*CH0 [23-16] = MSB (24 BIT DEVICE)*/ *ptr++ = SPI_RX_BUFF[4]; /*CH0 [15-08] = MID (24 BIT DEVICE)*/ *ptr++ = SPI_RX_BUFF[5]; /*CH0 [07-00] = LSB (24 BIT DEVICE)*/ *ptr++ = SPI_RX_BUFF[6]; /*CH1 [23-16] = MSB (24 BIT DEVICE)*/ *ptr++ = SPI_RX_BUFF[7]; /*CH1 [15-08] = MID (24 BIT DEVICE)*/ *ptr++ = SPI_RX_BUFF[8]; /*CH1 [07-00] = LSB (24 BIT DEVICE)*/ RECORD_H++; /*INCREMENT CIRCULAR BUFFER POINTER*/ if(RECORD_H == 32) /*CHECK FOR CIRCULAR BUFFER DEPTH*/ RECORD_H = 0; /*REST ONCE IT REACH TO MAX*/ } break; default: break; } } void ads1292R_Parse_Data_Packet(void){ if((ADS1292R_REGVAL[0] & 0x03) == ADS1292_24BIT){ ads1292R_Parse_Data_Packet(); } ECG_DATA_READY = 1; } void ads1292R_Device_Out_Bytes(void){ if((ADS1292R_REGVAL[0] & 0x03) == ADS1292_24BIT){ SPI_RX_EXP_COUNT = 9; /*3 BYTE STATUS + 3 BYTES CH1 DATA + 3 BYTES CH0 DATA*/ } }