Other Parts Discussed in Thread: ADS1292, ADS1292R
Hello,
I'm making a portable two electrodes ECG measurement system. We use standard dry AgCl electrodes. I would like to test our electrodes using the ADS1292ECG-FE demonstration kit. From the documentation I saw that the devkit is built for 4 electrodes ECG (ERA, ELA, ELL and ERL). Is it possible to configure the devkit for measuring an ECG signal using only two electrodes ?
For example, let's say I just want to use ELA and ERA electrodes, can I leave the ELL and ERL disconnected and read the signal from channel 1 (IN1P and IN1N) ? Or do I have to also connect the two others electrodes (ERL and ELL) ?
Could you please give me some informations on how to configure the ADS1292 registers for this type of setup (2 electrodes).
Thanks in advance for your reply