Part Number: ADC121S101
hi My customer would like to know why the current calculated is higher than measured at the input of the ADC (Vin) with 1Mhz SWITCHING CAP.
regards,
kamal
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADC121S101
hi My customer would like to know why the current calculated is higher than measured at the input of the ADC (Vin) with 1Mhz SWITCHING CAP.
regards,
kamal
Hello Kamal,
The numbers for DC Leakage Current in the datasheet (+/-1uA) are maximum limits for the device. The actual input leakage current will be less than this number.
Mike
there are three things that doesn’t fit:
Your expert: “The maximum input current at the input pin is +/-1uA”
My measurements: The input current is approx. -5uA when the input voltage is 0.5V, approx. 0uA when the input voltage is 2.5V and approx. 5uA when the input voltage is 4.5V. The ADC is supplied with 5V, and is running with 1Msps.
Your datasheet:
If you start with figure17: The sampling capacitor is charged to Va/2.
In figure16 the sampling capacitor with the initial voltage Va/2 is charged by the input voltage against Va/2. So the initial voltage of the capacitor and Va/2 in figure16 cancel each other and the input sees more ore less an empty capacitor.
This capacitor should have the capacitance of C_t=30pF according to your datasheet. The charging and discharging of the capacitor is repeated with fs=1MHz (aka 1Msps). So if calculate the input resistor R_in=1/(fs*C_t). (Details see here: https://en.wikipedia.org/wiki/Switched_capacitor )This gives you a resistor of 33k. If this resistor is right, the current would be linearly dependent on the input voltage and aprox. 30 times higher than I measured at 4.5V input voltage.
So what is right: your expert, my measurement or your datasheet.
there are three things that doesn’t fit:
Your expert: “The maximum input current at the input pin is +/-1uA”
My measurements: The input current is approx. -5uA when the input voltage is 0.5V, approx. 0uA when the input voltage is 2.5V and approx. 5uA when the input voltage is 4.5V. The ADC is supplied with 5V, and is running with 1Msps.
Your datasheet:
If you start with figure17: The sampling capacitor is charged to Va/2.
In figure16 the sampling capacitor with the initial voltage Va/2 is charged by the input voltage against Va/2. So the initial voltage of the capacitor and Va/2 in figure16 cancel each other and the input sees more ore less an empty capacitor.
This capacitor should have the capacitance of C_t=30pF according to your datasheet. The charging and discharging of the capacitor is repeated with fs=1MHz (aka 1Msps). So if calculate the input resistor R_in=1/(fs*C_t). (Details see here: https://en.wikipedia.org/wiki/Switched_capacitor )This gives you a resistor of 33k. If this resistor is right, the current would be linearly dependent on the input voltage and aprox. 30 times higher than I measured at 4.5V input voltage.
So what is right: your expert, my measurement or your datasheet.
HI,
Please find below the comment from my customer.
I do not see what can´t be determined if the datasheet tells the complete truth:
In hold mode the capacitor is charged with Va/2. In track mode this charge in the capacitor is canceld against Va/2 so the world outside sees an empty capacitor at the start of every track cycle.
If you charge an empty capacitor with Vin with the frequency fs the current is I=fs*C*Vin. In out case the current should be I=30uA/V*Vin.
Unfortunately I have measured something different. My current is negative (-5uA) at low Vin, zero at Vin=2,5V and positive (+5uA) at higher Vin.
For me this is a hint that the description of the topology in the datasheet is at least not complete.
regards,
kamal
Hi Kamal,
As mentioned in my post above you don't know the state of the sampling capacitor. The customer is assuming that the capacitor is completely discharged. It is not. The input of the SAR is very dynamic. See page 18 and 19 of the document slyp166.pdf at ti.com.
Mike
are you sure that the presentation is describing the ADC121S101?
The datasheet of the ADC121S101 says on page 12 in chapter 8.1:
“The control logic then instructs the chargeredistribution DAC to add or subtract fixed amounts of charge from the sampling capacitor until the comparator is balanced.”
So when comparator is balanced, the sampling capacitor has a voltage of -Va/2.
And as you charge the capacitor in track mode against +Va/2, the outside sees an empty capacitor.
This does not look like your presentation.
Please investigate how the ADC121S101 works.
Is the datasheet correct or the presentation?