Part Number: DAC37J84
Other Parts Discussed in Thread: TRF37T05,
My customer is seeing the following issues:
The DAC 37J84 was originally set to provide a full scale current of 30.16 mA by choosing a bias resistor value of 1.91 K.
The common mode voltage was 0.480 V when measured across one of the 50 Ohm resistors. Two 50 Ohm resistors were placed in parallel (one in front of the filter and another after the filter which is between the DAC and the IQ modulator (TRF37T05)).
I wanted to set the DAC full scale current to 20 mA. So I changed the bias resistor value to 2.94 K (results in19.54 mA full scale current). When I measured the common mode voltage, it was close to zero, and the power measured at the IQ Modulator output port was -65 dBm (before resistor change, it was around -20 dBm). Then, the 2.94 K was replaced by 1.91 K. it resulted in the values that were obtained originally. Then 1.94 K was replaced by 2.1 K and it yielded the same results as those of 2.94 K.
I would like to know why it works for only one resistor value that was originally selected for biasing the full scale current
I have a partial schematic and the results of the filter test if you want me to send them to you. Please let me know if you need them.
Thanks for your help with this!
Richard Elmquist