Part Number: ADS1220
Other Parts Discussed in Thread: ADCPRO,
I have a board of ADS1220evm, and I want to measure the temperature using 4-wire RTD when studying this development board. Because is a beginner, I don't understand, so encountered difficulties in connection, and, when using ADCPro, I according to clew input values, but the output data, I don't quite understand, read how to use the data to calculate RRTD on both ends of the resistance, which can draw the corresponding resistance, I in the development board R31 welding resistance value is 3.24 K ohm resistance, the R30 welding resistance of the resistance value of 0. and RTD has a resistance of 110 ohms,The development board is the one that just got it, there is a program, so there is no change in the program.The following is my connection mode, and the data read by ADCPro. What went wrong, please give a detailed explanation. I need your help very much. Looking forward to your letter, thank you.