When I was learning to use ADS1220, I tested with ADS1220evm, and my goal was to use 2-wire to measure the temperature of thermistor. The configuration is: R30 welding 0 ohm resistance, R3 welding 3.241K ohm resistance. In addition, I used the jumper cap to connect A3- and REF-, as well as A3+ and REF +, with a resistance of 110-ohm on both ends of the RTD. Wiring method as shown in picture, I am in the process of wiring series a current meter, if used to measure the flow of electric current is 500 microamps, but in the process of running ADCPro, I did not measure the current. I don't know what's going on here. Could you please give me some answers? Looking forward to your reply. thank your.