1. I supply the 5V power on AVCC and AVDD and DVDD, but supply 3.3V on IOVdd, is that a correct application?
2. When I measured the voltage on IOVdd, it is not 3.3V, it appears 4.2V, and when I cut off the connection from the IOVdd to 3.3V supply the Voltage on IOVdd pin is still 4.2V, but now the IOVdd pin get nothing to be connected, it looks the 4.2V come from the chip inside.