Other Parts Discussed in Thread: USB2ANY, PGA900
Hello.
I bought a pga900evm which comes with the usb2any. I suspect that the usb2any is not working & therefore I was wondering how I can order one of these? I cannot seem to find it anywhere online or on the TI website, which doesnt make much sense that I have to order the whole evaluation module again if just the USB2ANY is damaged? Please how can I exchange or replace this and get a working one?
The USB2ANY does provide power as expected when connected to the pga900 gu (Pin 6 of connector J4 on the USB2ANY board. Provides +3.3V. Pin 6 of connector J5 on the USB2ANY provides +5V). but I am unable to use it to change the registers or anything using SPI, OWI or I2C communication with PGA900EVM (I bought 2 extra PGA900 chips to make sure these were not the damaged ones.