Other Parts Discussed in Thread: ADS1263
The ADS124S06 advertises 4k Samples per second. However, I want to know what is practical SPS for measuring two inputs at two different frequencies. The primary measurement I want to measure as fast as possible. The secondary measurement is a temperature diode, and I only need to measure it occasionally (1-10SPS). I want to maintain a steady rate for the primary measurement, so I need to run the primary measurement at a speed such that the secondary measurement can be completed in between primary measurements. However, I don't see anything in the datasheet that specifies the time (or clock cycles) required to change between various settings needed to switch to the other measurement and back.
Details: One one set of ADC inputs (primary measurement) I am using one IDAC to drive constant current and measuring the voltage drop across a variable resistance network. I have a fixed resistor in series with this network, across which I am referencing my REFP and REFN. Occasionally (1 to 10 times per second) I want to switch to my secondary measurement, which is a voltage drop across a diode. I can enable both IDACs and the REF ahead of time (and leave them on), and since I have two IDACs I don't have to change the IDAC current setting (even if I had different currents). So really it comes down to switching to a different PGA gain, switching to the ADC inputs that the diode is attached to, changing the PGA gain, taking a reading (or 3 for the SINC3), switching the PGA gain to the primary measurement gain. What is the time required to do a secondary measurement and be ready for the next primary measurement? I'm using the internal clk of the ADS124S06. 3.3V to all supplies. No sleep or low power modes.