What is the max effective sampling rate for this reference design?
I see it is set to 4,915.2 samples per second but can it be increased/modified to achieve possibly something greater than 33,000
Thanks
Charlie A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the max effective sampling rate for this reference design?
I see it is set to 4,915.2 samples per second but can it be increased/modified to achieve possibly something greater than 33,000
Thanks
Charlie A
Hi Charlie A.,
I heard back from the team that designed TIDA-01094 and apparently the processor used there is not fast enough to support 33k samples. You would have to throw out samples.