This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8411: Oscillation of DAC when capacitor on output

Part Number: DAC8411


I have a Ferrite Chip Bead in series of the DAC8411 output, with a 100nF capacitor to GND, to form a LC filter.

Ferrite bead is 1500OHM @ 100MHZ. (HZ0402A152R-10)

The DAC8411 has a 100KHz Oscillation on its output, with the Capacitor connected. Nothing else is connected.

Shorting the Ferrite does not help at all, the oscillation is still there.

Is there any reason why this could happen?

Using a 1.5K Resistor and 100nF Cap works as a RC filter, but with the ferrite and Cap, the DAC oscillates.

The ferrite bead by itself, without the filter capacitor, also seams fine.

Any help appreciated

  • Hi Gerhard,

    The output of the DAC8411 string is internally buffered with an amplifier (see figure 74 in the datasheet), as such it can have issues with stability when there is a large capacitive load on the output. In fact if you look in the specification table of the device (pg 5) there is a specification called 'capacitive load stability' which is rated at 1000pF. Your load, 100nF, far exceeds that limit. When you add a series resistor to the output you isolate the output from the capacitor, which allows the internal amplifier to see a much smaller capacitive load.

    I would recommend you stick with the RC or buffer the output with an amplifier that can handle are large capacitive load.

    Thanks!
    Paul
  • Please mark 'This Resolved My Issue' if you have no more questions in regards to this issue.

    Thanks!
    Paul
  • Resolved by removing the Capacitor.

    Thanks