Part Number: ADS1115
Other Parts Discussed in Thread: OPA333, LMP91200, OPA2333, LMP7721
I am working on a design to allow connection of either ORP or pH probes to an ADS1115 in differential mode. The application is for aquaponics, aquariums, etc, so the inexpensive BNC connector probes would be connected to the circuit. The graph below shows an ORP probe in a 225 mV solution. The peak is where I was stirring the probe, and the falloff is from letting the probe sit in the solution. Since most of the probes produce +/- 1 V, I don't want to change the voltage, just produce enough current to prevent the signal from decaying so much when sampled. Is there an amplifier that might work well for this?
Thank you in advance.