This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32RF45: What source for configuration register settings should I use?

Part Number: ADC32RF45


The ADC32RF45 datasheet indicates that I should consult SBAA226 to obtain the (mostly undocumented) register settings that should be used to configure the device. I've seen links to it provided on this forum, but I've also seen many references to the GUI for the ADC32RF45EVM, which includes register settings of its own. It seems that the GUI settings might be more recently updated. Should I use those settings instead of those in SBAA226? It looks like there are some differences; for instance, SBAA226 has 3 different sets of IL configuration settings for each of the Nyquist zones, while the files bundled with the GUI has a single IL configuration section and only has differing Nyquist configurations for the NL configuration settings.