Other Parts Discussed in Thread: ADS127L01
Hello,
A customer has complained that GUI doesn’t connect to ADS127L01EVM.
I’ve confirmed bellow things with UG sbau260.
1) windows 7 32bits and Net Framework 4.6 used.
2) Core application and DVCPKG are installed correctly.
3) Generic Bulk Device driver, VID_1CBE and PID_003, is installed correctly.
4) Jumpers and switches on EVM are set up correctly as Table 2. Default Settings in SBAU261B.
5) Do UG 3.1 Startup Screen (No Hardware Connected) correctly.
6) Connect the EVM and then appear the GUI, title [Delta sigma Evaluation Software, but without ADS127L01].
7) For a while, some statements are showed on the bottom status bar.
Hardware Not Connected -> Unable to identify device= ADS127L01 -> Hardware connected,
but Register Map isn’t appeared, as image2.zip attached.
Let us know how to handle, please. I wonder ADS127L01EVM isn’t work correctly.
Regards,
Kazuo Yamauchi