Other Parts Discussed in Thread: OPA4180
Hi,
I am going to build a data acquisition system(DAS) with a precision of less than 0.05%, I want to choose ADS8688A which has a 16 bits resolution. But in the file " tidu365b.pdf" a projest is provided, which shows that the accuracy over entire input range is 0.2%(much higher than 0.05%). So is there any other ADC recommended?
I have another two questions about the file " tidu365b.pdf" .
1 In the file " tidu365b.pdf" , figure 26 to figure 31 show the test accuracy results, how is the FSR(full scale range) Error calculated ? For example, there are two groups of datas for an analog input, group one is tested by a multimeter, group two is the output of ADS8688A, so how can we calculate the FSR Error with the two groups of data ?
2 In the figures we can see the FSR Error is much smaller after calibration, so what is the exact method of calibration ?
figure 26 to figure 29 are shown bellow: