Part Number: ADC12J4000EVM
Other Parts Discussed in Thread: ADC12J4000, ADC12DJ3200, LMX2581, LMK04828
Hello!
I'v got adc12j4000EVM rev.E3 and I try to connect it to my vcu108 xilinx board. Bypass mode 3760 Msps.
According the datasheet for this ADC I am using following parameters for jesd(xilinx jesd 204b ip core v7.1) - for default parameters from adc gui:
F=8
K=4
L=8
LineRate = 7.52Gbps
ReferenceClock = 188MHz
SYSREF on Positive Edge
Using global clock 1
scrambling on
sysref always on
sysref required on re-sync
In additional transceiver control ports I'v changed polarity for gt_rx ports; In ADC gui v1.1 I press button "program clock" in bypass mode; And for test I am turning on Short/Long transport test.
So I expect to see rx_frame_error bus all zeros and the sequence on output bus.
But I have infrequent errors. What may be the reason of such problem.


(block design and chip scope print in attachment)