Part Number: TSW14J56EVM
Other Parts Discussed in Thread: DAC38RF82EVM
Hello,
I have successfully managed to generate an arbitrary waveform using the TSW14J56EVM and DAC38RF82EVM. I have also managed to trigger the start of the waveform generation using J13 on the TSW14J56EVM.
However, for my application, I need to be able to precisely trigger the start of the waveform many times per second. If I am correct, J13 is not currently set up to do this. It can only trigger the start of the waveform once and then I must "Write DDR Memory" again either from the HSDC GUI or from MATLAB or C to "reset" the system.
Is there an option to set the trigger to have this functionality that I am missing? If not, what steps need to be taken to add this ability.
Thank you for you help!
Matt