Part Number: DAC8750
I have my first run of product using the DAC8750. While all prototypes function correct, I have a few where SPI data does not go through. In my code I continually update the control, config and DAC registers about once every 1.6mS. If you put a scope probe on the clock line it starts working. Viewing the scope waveform from one that works vs one that does not appears the same. The SPI lines are directly connected to the host micro. I am running the SPI clock at 16MHz (no change if I back it down to 4 MHz).
These were assembled by hand. Any chance of damage from assembly or do I have an electrical issue that is right on the edge ??