Part Number: ADS1232
Good morning to everyone.
We use the ADS1232 AD since 2007 and it’s very good for our balances application. Suddenly, in our production, we have a serious problem to the power on reset.
We didn’t change anything both in the hardware and in the firmware. But now, at the beginning of the power on the converter sometimes and random seem to be locked. And nothing can be done to unlock it. Only another, power on reset directly from the power supply unlock it. This strange condition it isn’t systematic. On the same board 6-7 times appear but not in all production. But the total percentage is a bit worrying.
I checked components, values, board and all seem to be right. Even the pin N° 22 PWD has a RC filter about 1 ms.
I never had any problems like this and I hope someone can help me. If it was necessary I can give more details.
Thanks a lot.
Claudio