This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW1400EVM: Max. Sample Rate for Dual Channel ADC

Part Number: TSW1400EVM
Other Parts Discussed in Thread: ADS5407, ADS5402, DAC3283

Hello,

does the TSW1400EVM support a sampling of two channels with a sample rate of 500 MSPS each and a bit resolution of 12 Bit like it's necessary for example  for the ADS5407. In the desciption I can find that it provides 16-bits of data at 1.5 GSPS. However, in the User's Guide of the TSW1400EVM  I found the information "For two-channel parallel DDR bit-wise data formats, 14 of the LVDS data pairs are used to support two channels of 14-bit resolution at up to 250-MHz sampling rate." How do these two informations fit?

 

Best regards

Benjamin