This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131A04EVM: do we need to buffer the input signal before connecting to the ADC pins

Part Number: ADS131A04EVM

In the ADS131A04EVM board, do we need to buffer the signal before connecting to the ADC pins ?

My sensor is a simple wheastone bridge). Without EVM, sensor outputs 4 mV. When EVM is connected, the output is changing to 9mV

Does the ADC has an internal Buffer to prevent loading ?

Regards,