Other Parts Discussed in Thread: PGA970, USB2ANY
Hi,
We have purchased PGA970EVM to evaluate PGA970.
The GUI software and the necessary LabVIEW are installed as per the procedure.
After connecting the EVM through USB2any, the GUI recognizes the board and the
Hardware is Connected properly. All the jumper connections are at default state(Factory Setting)
VDD Selection Jumper set to VDD_OWI(also tried connecting only VPWR).,
But we are not able to get any of the analog(ADC/DAC) working.
READ ADC(ADC1 data) is all Zero.The temperature sensor is also zero.
Is it required to program the EVM befor connecting to the GUI?
Is there anything else to be done to get proper reading from PGA970EVM?
The power supply seems OK.. all the Test point voltages a seems goood.
Have tried with the same settings mentioned on this E2E and also with
two different PCs, but no success.
https://e2e.ti.com/support/sensor/pressure/f/998/t/577226?tisearch=e2e-quicksearch&keymatch=PGA970EVM
Regards
Paddu