Hi,
I have a few questions regarding the communication between the ADS1299-4.
While checking for the communication between the IC and Arduino , I have tried to read some register values first. - See the attachment
Q1. I would like to conform if the ID register value I am getting is correct or incorrect.
I am getting 0xDF instead of default 0xXC (according tho the datasheet), while the other registers return the default values.
Is the device is faulty?
This question is related to - e2e.ti.com/.../602946
Q2. I am unable to write to any registers, while I could read them. (even after writing, the register values remains same as default value) is it because of the Voltage values are incorrect or the IC is faulty?
PS. The capacitor voltages with respect to GND are given below.
DVDD : 3.3 V
AVDD : 2.5 V
AVSS : -2.5 V
VCAP1: -1.2 V
VCAP2: 0.0 V
VCAP3: 1.8 V
VCAP4: -2.5 V
Attachments -
Thank you.