Part Number: DAC8775
Hello team,
Please find customer issue below:
**************************************************************************
I'm testing the board and I find that the accuracy depends on the load you put on the current loop. I must be doing something wrong.
This is the configuration I am using:
Measured results:
Code 152Dà
Shortcircuit -20.000mA
160ohms -19.890mA
470 ohms -19.681mA
As you can see, the result is different depending on the load. Could you please help?
**************************************************************************
Thanks and regards, Jose