Part Number: ADS8363EVM
Other Parts Discussed in Thread: ADS8363
Hi
I am using ADS8363 EVM ,the jumpers for M0 and M1 are open stating automatic mode and through SDOA only ,now I was trying to sample data in from same voltage source in two different channels but getting different result.One channel is giving correct result.(when running with breakpoints in debugging mode).But still some times it also gives wrong results.(when running directly without any breakpoints in debugging mode). I am using host MSP430F5529LP. Checking the value stored in array in mV after conversion and post processing.I am unable to find its reason.I am also writing the SDI in beginning to turn on REF1 DAC ,by checking using multi-meter i am able to see 2.4 V at that pin on EVM, suggest what may be possible issue.
(Ignore any typo mistake).
PS:also I wanted to work in psedo diffrential mode in mode 4 ,but I am not clearly able to get how to implement that,as its automatic so we need not be definig channel sequence .Plaese also show some light on that .
Edit:1
I checked the analog input voltage at chip also its coming same,also I have assumed it in fully differential mode and grounding the -ve terminal of differential input to ground.
Regards
Anmol