Part Number: ADC3421
Hello team,
I have two quick questions about the sampling rate for the ADC3421:
1. The max sampling rate is 25-MSPS. Since this is a four-channel device with four ADCs, does this mean that each of the four internal ADCs can sample at 25-MSPS, or would I need to divide that rate by 4?
2. Is it possible to have the internal ADCs sample at different rates? E.g. have channel A sample at 20-MSPS and have channel B sample at 15-MSPS?
Regards,
I.K.