Part Number: ADS1299
Hi there,
We've been using the ADS1299 to get some EEG signals but we've not been sucessful. Either because of the electrodes or the hardware configuration, we just seem to be a bit off. Hence, I'd like to get some answers that may point us in the right direction:
1) In the datasheet, you recommend a differential capacitor across the positive input and the negative input of channels and, when a reference is used on SRB1, a differential capacitor between the positive input and the reference, instead of RC filters on every input. With this configuration, the signal we get is simply just noise and there's no EEG, EMG or ECG signal whatsoever. But, when we do change to single RC filters on every input, we can see ECG, EMG but not EEG. The channel outputs are a bit noisy, not as much, but the channels used to read EEG don't actually show anything. So my question is: Using a RC filter on every input and a single ended input, we need a RC filter on every positive input and just one RC filter on SRB1 right ? What about the negative inputs? When we activate SRB1 they should all shunt together, but any resistors or caps on those lines will affect this schematic ?
2) The RC filters on the inputs are antialiasing filters. What should be the cutoff frequency of those filters? And what is the minimum value for the input resistor ?
3) How can we guarantee that the noise on channels are not compromising an EEG signal ? Is there any test we can do ? We have an EEG simulator and we can read (although it is a bit difficult) sine waves with 10uV of amplitude.
4) We can also use the off band lead off detection, but we can't get a clear resistance value when we choose the 6nA option. The values seem to "float" up and down endlessly, although they change quite a bit (from 6MOhm to 110kOhm) when the electrodes are connected. Is this an indication that something might be wrong along the way ?
5) We're using the OpenBCI schematic on the BIAS pins (1MOhm and 1.5nF capacitor on the BIAS OUT pin connected to a protection resistor of 5kOhm and then to the electrode) and, although it reduces alot the noise on the channels, it can't completely remove it. After that, we apply two digital filters: notch filter on 50Hz (-45dB) and a butterworth bandpass (0.1Hz to 80Hz - -10dB). Could these filters be interfering in some way with the results ?
We've been going back and forth with the schematic of the ADS1299 and sometimes it's really easy to capture EMG signals, specially the eye blink. But even then, we get no results when it comes to EEG. We're using dry active electrodes. The circuit of the electrodes has been tested separately by applying the simulator output to them and checking the output of the ADS1299. The electrodes themselves are being used on other commercial applications and work fine. But something in this mixture is not cooking correctly.
I'd appreciate any help from you guys.
Luis