Other Parts Discussed in Thread: ADS1178
Hello.
I am looking to develop a device in which the analog measurements are synchronized on UTC. The goal is to have several devices with analog measurements that are synchronized at +/- 100ns. Imagine that we have a 10MHz clock perfectly synchronized on UTC (using a GPS chip) and that the /SYNC pin of the ADS1174 in each device are synchronously pass from the low state to the high state using a pulse also synchronized with UTC. Will the samples of the ADS1174 be synchronized? Will the samples stay synchronized for a long period of time (several days, that is the question for the reliability of the clock chain)?
Thank for your help,
Best Regards