Part Number: ADC083000
Hello,
I'm using the WaveVision 4.3.01.5 Beta ADC08X3000 Software and want to customize it. I have a few questions about customizing this software.
a) Can I customize this software with the IDE such as Eclipse or NetBeans? If I can, I want to know about the following:
・The version of the IDE that is available
・The way to import software files into the IDE
b) I checked the contents of the folder named "WaveVision", but I don't know what features each class file implements. Which class file contains the code to acquire data from the ADC when the "Acquire" button is clicked? I want to customize this software to increase the measurement number at once or to repeat the measurement several times continuously.
Best regards,
M.T.