A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
RCV420: 4-20 mA current loop receiver with multiple input channels
The RCV420 is the only integrated 4-20mA receiver we offer and we do not have a 4-channel version of the device.
What are the requirements of the application? If you do not need to continuously receive data from each of the current loops at the same time then you could consider using a multiplexer in front of a single receive circuit.