Part Number: LM15851
Other Parts Discussed in Thread: TMP421, DXP
Hi
I'm using TMP421 with LM15851 for reading the temperature. It reads negative temperature (like -40 °C) for the remote sensor that is connected to TDIODE+/TDIODE- of LM15851. The local sensor is okay.
Also I have another TMP421 connected to a MMBT3904 and another one to a Xilinx FPGA, both remote and local temperatures of them are correct. So I'm sure that the problem is not the software.
How can I fix this problem? Should I use n-Factor Correction or something?
Regards,
Robert