Hello,
I was working for some months with electrochemical gas sensors typically from Alpha Sense company which require an analog front end to be designed. Until now I did some prototyping and I have created some AFE using operational amplifiers and other passive components. Lately I ran on the LMP91000 chip from TI and seems very nice especially for 3 pin electrochemical gas sensors. Until now I used the A4 sensors from alphasense and I did not considered this chip also from the fact that those sensors have 4 pins and an external operational amplifier was required in addition to the LMP.
In this moment I need to use sensors from spec-sensors.com which are 3 pin and LMP91000 can be used, but those sensors also have a smaller output current typically 4.5-20 nA/ppm. I need to be able to measure tens of ppbs therefore I suppose I need a big amplification. Moreover I need to have 4 of them on a single board. Alongside with the 4 LMP91000s I want to use a 24 bit ADC to convert the output of the AFE into numerical form. I have found the following ADC from TI: ADS1226 which has 2 differential channels therefore for 4 sensors I will need to use 2 of them and LMP90100 which has 4 differential channels and also another PGA inside which, I think, will help with the amplification.
Last note that I want to mention is that I am not an electrical/electronic engineer, but a computer science one and therefore I have limited knowledge of analog design.
My questions are: is the LMP91000 suitable for those sensors(from spec)? Is the LMP90100 ADC the better choice to go along with LMP91000 AFE or should I seek another one? Any other guidance when using such sensors is welcome.
Thank you!