Part Number: ADS8881EVMV2-PDK
Other Parts Discussed in Thread: ADS8881, ADS9110
Hi, I have a question about the resistance accuracy in the BOM of ADS8881 EVM2.
As you can see, R13/R16, just has 1% accuracy, which means the gain error of this stage is around 1%, greatly high than 1 LSB requirement.
I think this greatly degrade the DC performance, makes the high resolution of ADS8881 and high accuracy of REF useless?
I also checked ADS9110 EVM, the resistance accuracy is 0.1%, also doesn't fit the LSB accuracy.
So could you please tell me how to calculate the DC accuracy of ADS8881 EVM?
Thanks.
Marc