Part Number: ADC3222
Hi,
I am using ADC3222 in my receiver design and I encountered a problem:
The input signal is a baseband signal (I/Q data) with symbol rate of 400 kHz and the sampling clock frequency is 21 MHz
I have performed few tests and it looks that the noise floor of the sampler is high:
1) Using a CW signal at 10 ÷ 80 kHz at -24 dBm and SNR bigger than 25 dB I get SNR of ~10 dB (the SNR encountered at 10 kHz and 80 kHz is the same, so it did not look like a sampling clock jitter problem).
2) Grounding the I/Q input pins of the components I see ~5 digital bits changing with time.
3) Using a CW signal with SNR of 6 dB at -4 dBm dB I get SNR of ~6 dB
I will appreciate if you can help improving my design.
Thanks,
Shlomi