This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ3200EVM: External clocking at 4GHz and DC coupling

Part Number: ADC12DJ3200EVM
Other Parts Discussed in Thread: ADC12DJ3200, , LMH5401, LMH3401

Hi,

 

I have a couple of questions about the ADC12DJ3200 and it's evaluation board capabilities.

 

  1. The ADC12DJ3200 datasheet specifies a sampling rate of 6.4Gsps in single mode operation, however, the maximum clock frequency is specified as 3.2GHz. Is the 6.4GSps achieved through internal engineering? Does that mean a 4GHz clock cannot be used to achieve a sampling rate of 4Gsps?

2. We would like to DC couple our input signal to the ADC12DJ3200EVM. Are there any modifications that need to be done to the eval board? Also, do you have a recommended differential amplifier that has a flat gain over the entire 8GHz bandwidth?

Thanks,

Apurva S. Gowda