Part Number: ADS1293
Hi,
I saw the isolation solution as below
If I power the system by AC-DCs, Can I use the solution?
Or can I isolation the ECG system at the PC interface if I power the system by AC-DCs?
I want to design a ECG system with lead 3, lead 4, and lead 5. Can I use ADS1293 to finish it? Do you recomand AFE or other discrete component solution?
I need the anolog ECG signal. Can I get the signal from ADS1293, and change it into anolog signal with DACs?
Best regards,
seven