Does TI have an algorithm description or software for calculating the "I/Q Offset Adjust", "I/Q FSR Adjust", and "DES Timing Adjust" from sampled data? If so, are they willing to share it with customers?
I'm recording a nearly full scale tone in DES mode. The tone is phase locked to the sample clock generator. Therefore, the frequency of the sampled data exactly matches the frequency programmed in the signal generator. I choose a frequency that will produce an integer number of cycles in the recorded data. I'm working on an algorithm that will automatically calculate the above mentioned register settings for optimal spur mitigation, but it would be nice if TI already has an algorithm they are willing to share.
Regards,
Scott