This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC3164EVM: DAC3164EVM - FMA DAC Adapter Card Signals

Part Number: DAC3164EVM
Other Parts Discussed in Thread: DAC3162EVM, DAC3162, DAC3164

Kindly see the Schematics of the DAC3164EVM and FMC-DAC Adapter Card (Both are TI make).
Also, see the DAC3162EVM Schematics.
The Webpage of both the EVMs' (DAC3164EVM and the DAC3162EVM) say that they are compatible with the FMC-DAC Adapter Card. 
In the Schematics of the DAC3162EVM, the Interface Connector signals match to those on the FMC-DAC Adapter Card, in terms of numbers (1 to 172) and "Nature".
Whereas, in the Schematics of the DAC3164EVM, the Interface Connector signals DO NOT match to those on the FMC-DAC Adapter Card, in terms of numbers (1 to 192) and "Nature". See the Pin 118 of the Interface Connector of the DAC3164EVM. It is FPGA_ClockOutN. This pin on the FMC-DAC Adapter Card is an NC  EmojiEmojiEmoji.
Kindly let me know how do I use the DAC3164EVM with the FMC-DAC Adapter Card, which is what the webpage says.