This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7952-Q1: ADC sampling accuracy for ADS7952

Part Number: ADS7952-Q1
Other Parts Discussed in Thread: ADS7952

HI,TI

In the process of using ADS7952, I found that his sampling accuracy was very poor, as shown in the table, the error was unacceptable

输入电压
CH11 理论换算 实际读取 实际采集值 CH10 理论换算 实际读取 实际采集值
0.837 169.2414 161.7 0.799703264 135.594 135.8 0.838271605
1.151 232.7322 222.4 1.099901088 186.462 187 1.154320988
1.513 305.9286 303.3 1.5 245.106 245.4 1.514814815
1.934 391.0548 384.2 1.900098912 313.308 314.4 1.940740741
2.411 487.5042 485.3 2.400098912 390.582 392.1 2.42037037
2.708 547.5576 545.9 2.699802176 438.696 441.1 2.722839506
3.172 641.3784 626.8 3.099901088 513.864 515.5 3.182098765
3.735 755.217 748.2 3.700296736 605.07 606.5 3.74382716
4.236 856.5192 849.3 4.200296736 686.232 667.5 4.12037037

clipping

  • Hello Clipping,

    Welcome to the TI E2E Forum !

    The ADS752 operates in two possible Vref range settings. I am not able to match your theoretical conversion to either range. Could you please share the measured Vref reference voltage and the Range setting used in your design?

    Thanks.

    Regards,

    Sandeep

  • Thank you,Sandeep!

    I know why it wrong,Data type conversion leads to distortion.

    Next question:I have about 400mv burrs on GND, which causes the ref-voltage to also have burrs. How can I filter the hair out?

    I use REF5025 chip.

    Clipping