This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1293: ADS1293 can not support AAMI EC11、EC13、IEC60601-1、IEC60601-2-27 and IEC60601-2-51 standards ?

Part Number: ADS1293

Dears,


our client find the ADS1293, but spec did not show  AAMI EC11、EC13、IEC60601-1、IEC60601-2-27 and IEC60601-2-51 standards support?


is mean cannot support standards?  or H/W design can do for help?


If our need design lead 5 ECG application, have any suggestion part number?


If any, please advise me.


Thanks,


Best regards,


Lawrence.