This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a 14-bit ADC. However, looking at the datasheet , the effective number of bits (ENOB) is always less than 12 bits.
Why is my the ADC claiming to be a 14-bit ADC when it only has 12-bit accuracy? What is the point of having two extra bits if they are meaningless?
When calculating 1LSB do I need to consider resolution as 12bit or 14bit. When we will get full resolution 14bit from ADC.
Regards
Hari T O
Hello Hari,
Please refer to my references in your accompanying E2E post: https://e2e.ti.com/support/data_converters/etc_data_converters/f/77/p/642718/2370316#2370316 . These will apply here as well.
Regards,
~Leonard