Hi,
I am using ADS1299 for EEG measurement. EEG data which i captured is ok. but when i captured real time impedance on patient body then it gives some error.
each time when i connect a new electrode on my board the value of the previous channel impedance increase by one, same happened when i connect 3rd electrode the impedance of first and second electrode increase by one. so overall if i connect 10 electrode then the impedance vary on the first electrode is (impedance when First is connect +10). i don't understand such type of behavior of the chip.
I used 6 uA and 7Hz frequency for impedance measurement.
if some one know about this problem then please help me.
Thanks and Regards