Part Number: ADS1120
Other Parts Discussed in Thread: , ADS1220
Hi TI team,
My product is used ADS1120. Does ADS1120EVM have code? Many thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hardy,
Unfortunately we do not provide the source code for the ADS1120EVM, but we do have some basic code for the ADS1220 which is the 24-bit version of the device. This is pretty much the same as for the ADS1120 with the exception that the data for conversion results are 16-bit instead of 24-bit.
http://www.ti.com/lit/zip/sbac227
The EVM software uses the USB peripheral and enumerates as a communications device class (CDC) creating a virtual COM port on your PC. The EVM software is very much like the MSPWare example for CDC with communication through a COM terminal like HyperTerminal or Tera Term. So you can add the example files for the ADS1220 into the MSP CDC example project.
http://www.ti.com/tool/mspware
Best regards,
Bob B