Part Number: DAC161S997
Hi team,
A customer has problems about his PCB, the details are as follows, could you please help? Thank you!
DAC161S997 is used to design a 4-20mA driving circuit. The PCB is designed according to the schematic of DAC161S997EVM. All the chips are same except the power supply chip. Here arehe problem:
1. When powered up, the current is 80mA; the base voltage of triode3904 is 2.7V, what may cause it?
2. The output of LDO is normal, the external supply voltage is 12V, the voltage on one side of D1 is 12V, while the other side is about 8V, D1 becomes hot soon, what may be the reason?
Sincerely,
Hao