Other Parts Discussed in Thread: ADS1248
Hello There,
I am having a problem measuring all analog intput using the multiplexer. I am using a Ratiometric principle, but instead of a 3-wired method, i have all analog input connected. Talking about like 6-wire principle, permit me to say so ;-)
Each time i conduct sampling of all channels using the multiplexer to interchange the channels, i get an error of about 7% in all sampled channels except the first channel.
If i disconnect all channels(take out all PT-100 Resistors ), leaving only one at a time while sampling, then i get values without the 7% error.
Possible Problem:
There could be a leackage of current through the other analog input channels when connected, even while no current flows through. Is this current able to course the 7% error?
Somebody help me out.