Part Number: DAC80004EVM
Other Parts Discussed in Thread: DXP
Got the DAC80004EVM. If I correct its required also the MMBO board too.
Is it correct?
How to order it?
The related s/w tool is the DXP DAC Exerciser Program?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC80004EVM
Other Parts Discussed in Thread: DXP
Got the DAC80004EVM. If I correct its required also the MMBO board too.
Is it correct?
How to order it?
The related s/w tool is the DXP DAC Exerciser Program?
Eli,
The DAC80004EVM is designed with the HW form-factor that can interface the MMB0 / DXP platform, although the kit does not include an MMB0 (essentially this was to reduce cost of the kit and make it more accessible).
If used with DXP a configuration file will be required which is attached to this post.
Most likely the quickest method to acquire a MMB0 board is to order an "EVM-PDK" which includes the MMB0 given import / export control restrictions with respect to shipping.
<?xml version="1.0" encoding="utf-8"?>
<device>
<name>DAC80004</name>
<revision>1.0.0</revision>
<date>6Jun2014</date>
<devicesettings>
<instructionwidth>32</instructionwidth>
<format>sbinary</format>
<dataword>XXXXCCCCAAAADDDDDDDDDDDDDDDDXXXX</dataword>
<commanddefault>0</commanddefault>
<commandlatch>3</commandlatch>
<maxupdaterate>1000000</maxupdaterate>
<channels>4</channels>
<interface>
<type>spi</type>
<polarity>0</polarity>
<phase>1</phase>
<maxsclk>50000000</maxsclk>
<framebits>32</framebits>
</interface>
<latchpin>
<feature>1</feature>
<pulsepol>0</pulsepol>
</latchpin>
<FSplus>4</FSplus>
<FSminus>0</FSminus>
</devicesettings>
<gpiofunctions>
<function>
<gpio>5</gpio>
<name>Clear</name>
<default>1</default>
<active>0</active>
<labels>
<active>CLEAR</active>
<inactive>notcleared</inactive>
</labels>
</function>
</gpiofunctions>
</device>