Part Number: DAC161S997
Other Parts Discussed in Thread: DAC8750, DAC8775, DAC8760
Hi all
We are making a PLC with several I/O and the analogs outputs are driven by the DAC161S997
The problem is the connection of these outputs, we are using a 24VDC power supply to power the loop, and a 3.3VDC to power the digital side. These two have a common ground, so when we connect the loop supply, the DAC gets hot and the current in the loop goes to 40 mA.
To avoid this, we separated the grounds so the 24VDC runs alone in the loop and the 3.3V powers the DAC.
We observed this was the only way the DAC worked properly.
But when we connect a 24VDC actuator, it doesn't work because this one connects internally the 4-20mA input ground to the 24VDC supply (as expected)
Another Issue we have is to connect multiple DACs, we have 4 analog outputs and we only can use 1. Since we have only one 24VDC power supply we cannot connect the 4-20ma loops in paralell because when we make the ground common the DACs won't work properly.
So, if we want to work we these outputs we need to have one 24VDC supply separately from each loop and at the same time the power in the loop cannot be common with the 3.3V DAC supply, A real nightmare!
We have rechecked the connection several times and it is the same provided in the datasheet:
I appreciate any help with this, we have tested everything with the same result.
Thanks