Part Number: ADS8688A
Table 14 of the ADS8688A datasheet shows 16 bits of data written in to the ADS8688A and 16 bits read from the part as detailed in Figure 91 (and Figure 100 and 102).
Setting the "SDO data format bits" in the Feature Select Register then continues the SPI transaction with 9 more bits read from the ADS86888A. So if I understand this correctly, the total SPI transaction is 41 bits long.
Can the transaction be cut short--say at 40 bits (an 8 bit boundary) without causing troubles, just the final bit not sent?
Or could the transaction be extended to 48 bits? Would the ADS8688A simply hold SDO low during the extra SCLKs?
Thanks,
Bruce